8 Different Types of Signal Generators: A Comprehensive Guide for Electrical Engineers

Your browser limits use of the Used Keysight Equipment website.
Please consider switching to a current version of Chrome, Firefox, Edge or IE11 to use this site.

Have you ever found yourself troubleshooting a complex electronic circuit, only to realize that your signal generator isn't up to the task?

Imagine working on a cutting-edge radar system, where you need to simulate a variety of real-world signals to ensure robust performance. 

Selecting a high-quality RF Vector Signal Generator, instead of a basic Function Generator, could mean the difference between hours of frustrating diagnostics and a smooth, efficient validation process.

In the worlds of electrical engineering, electronics, and communications, signal generators don't just assist; they command the stage. They provide the test signals you rely on to dissect, analyze, and fine-tune your components and systems. Choosing the right one can elevate your project from a headache to a success. 

In this guide we will dive into a selection of 8 signal generators, giving you the knowledge to unlock the full potential of your next project.

The Signal Generator and Its Pivotal Role in Modern Electrical Engineering

At its core, a signal generator serves as the maestro of electronic testing, directing a symphony of signals that breathe life into circuits and systems for evaluation. 

It creates controlled, precise waveforms of varying types—be it sine waves, square waves, or complex modulations—to test, validate, and troubleshoot electrical setups. Without signal generators, you'd be flying blind, with no reliable way to simulate how circuits respond to different types of inputs.

Picture yourself fine-tuning a high-fidelity audio system, debugging a digital communication channel, or even developing next-gen radar tech; in each of these scenarios, a signal generator becomes your trusted partner. 

A signal generator mimics real-world conditions, whether you're dealing with audio frequencies, digital patterns, or radio waves. From basic component testing to advanced research and development, a signal generator is your indispensable partner in problem-solving and innovation.

Find Keysight Signal Generators On Sale
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
Essential Features and Specifications

Understanding the essential features and specifications of a signal generator is like knowing the ingredients in a recipe; you can't achieve the end result you desire without the right components. With that in mind, let's look at what you should consider when selecting your ideal signal generator.

Essential Features and Specifications

  1. Frequency range: This element is crucial for defining the variety of tasks your signal generator can tackle, be it low or high-frequency applications.
  2. Modulation capabilities: To mimic real-world conditions effectively, your signal generator should support a wide range of modulation schemes, from AM and FM to more intricate digital modulations.
  3. Output power: Adequate and adjustable output power lets you drive the system or circuit at varying levels, making it essential for stress tests and other evaluations.
  4. Resolution: Higher resolution means more accurate test results, allowing you to dissect and understand your system or circuit with greater precision.

Using high-quality, calibrated signal generators, like those from Keysight, offers a level of reliability and accuracy that can make a substantial difference in your work. These professional-grade devices undergo rigorous testing and calibration, ensuring that the signals they generate are both accurate and consistent. 

Skimping on quality could lead to erroneous results, potentially setting back your project and increasing costs in the long run. Make the wise choice; your project's success could depend on it.

Different Types of Signal Generators

Understanding the variety of signal generators and what they can do is paramount. Each type has its own special capabilities and uses, making your work easier and more effective. 

Let's delve into the first of these invaluable tools to better understand how they contribute to the world of electrical engineering.

1. Waveform or Function Generators

A waveform or function generator is a device that produces simple, repetitive waveforms. These generators are the go-to devices for basic testing and troubleshooting in various engineering applications, be it in electronics, mechanics, or even physics.

Typical Waveform Shapes and Their Applications

  • Sine wave: Used for testing linear circuits and systems, like audio and RF amplifiers.
  • Square wave: Essential for clock signals and timing analysis, often used in digital circuits.
  • Triangular wave: Useful in applications like voltage-to-current conversion tests and integrator circuit assessments.
  • Sawtooth wave: Employed in applications like sweep testing and video signal generation.

Real-World Application

One critical application for waveform or function generators lies in educational settings. Engineering students use these devices to learn the fundamentals of circuit analysis and electronic design. 

Whether it's creating a sine wave to understand oscillatory behavior or generating a square wave to learn about duty cycles, the function generator serves as an invaluable teaching tool. 

It simplifies complex theories into observable phenomena, making it easier for aspiring engineers to grasp the building blocks of their future professions.

2. Arbitrary Function Generators and Arbitrary Waveform Generators (AWGs)

Arbitrary function generators and arbitrary waveform generators (AWGs) are the chameleons of the signal generator world. While standard function generators are limited to basic waveforms like sine and square waves, these devices give you the flexibility to create both standard and intricate custom waveforms. 

Whether you're simulating a cardiac pulse in medical research or generating complex modulations for telecommunications, these generators offer unparalleled versatility.
 

Primary Differences and Advantages

FeatureFunction GeneratorArbitrary Waveform Generator (AWG)
Standard WaveformsYesYes
Custom WaveformsLimitedExtensive
ComplexityModerateHigh
Memory DepthLowerHigher
Update RateSlowerFaster
CostGenerally less expensiveGenerally more expensive

 

Real-World Application
In the world of telecommunications, arbitrary waveform generators (AWGs) play an essential role in testing and developing 5G networks. They can generate the complex modulated signals needed for 5G, allowing engineers to simulate a range of conditions that a 5G network will encounter. 

This capability is crucial for ensuring that the network can handle real-world scenarios efficiently and reliably, accelerating the development and deployment of next-generation communication technologies.

3. RF Signal Generators and RF Vector Signal Generators

RF Signal Generators and RF Vector Signal Generators

When it comes to radio frequency (RF) testing, RF signal generators and RF vector signal generators are your mainstay tools. 

While both types produce RF signals, vector signal generators go a step further by adding complex modulations to the carrier wave. This functionality enables more realistic simulations, especially important for modern digital communication systems.

Key Features and Applications

  • Applications: From mobile device testing to radar systems, these generators are invaluable in a wide array of RF applications.
  • Frequency range: Typically spans from a few kHz to several GHz, covering most commercial and many specialized RF bands.
  • Modulation capabilities: Basic RF signal generators often handle AM and FM, while vector versions can modulate advanced digital schemes like QAM and QPSK.

Real-World Application
RF vector signal generators find critical use in the aerospace and defense sector, particularly in the development and testing of radar systems. Their ability to generate signals with complex modulations allows for realistic scenario simulations. 

For example, they can emulate the signal reflections off a moving aircraft, helping engineers optimize radar algorithms for tracking and identification. This precise testing is vital for ensuring that radar systems will perform reliably when deployed in real-world situations.

4. Pulse Generators

Pulse generators specialize in creating digital pulses, making them indispensable in the realm of digital circuits and communications. Unlike waveform generators, which focus on continuous signals, pulse generators excel in creating discrete, time-bound pulses. These pulses serve as the lifeblood of digital systems, facilitating clocking, synchronization, and data transfer.

Key Features

  • Pulse width: Defines the duration of the pulse, critical for timing accuracy in digital systems.
  • Rise and fall time: Specifies how quickly the pulse reaches its maximum and minimum values, essential for minimizing signal distortion.
  • Repetition rates: Indicates how frequently the pulses occur, influencing the throughput of digital systems.

Real-World Application
Pulse generators play a crucial role in data storage technologies, especially in the quality assurance of solid state drives (SSDs). These generators produce the digital pulses used to read and write data, simulating various conditions that the SSD might encounter.

By adjusting parameters like pulse width and repetition rate, engineers can rigorously test the SSD's performance, ensuring that data read and write occur swiftly and reliably under different scenarios.

5. Video Signal Generators

Video signal generators take center stage in the domains of television, broadcasting, and video testing. They create a variety of video signals that mimic real-world scenarios, helping to calibrate, validate, and troubleshoot video equipment and displays.

Key Features and Common Use Cases

  • Formats supported: These generators often support a wide range of formats, including NTSC, PAL, and HD, making them adaptable for various broadcast standards.
  • Common use cases: Calibration of display monitors, quality assurance of video codecs, and stress testing of broadcasting equipment are among the variety of tasks these generators handle.

Real-World Application
In professional sports broadcasting, video signal generators are indispensable for ensuring a seamless viewing experience. 

Before a big game, engineers use these generators to test all video equipment for errors or inconsistencies, ranging from cameras to transmission systems. 

This preemptive testing ensures that millions of viewers enjoy a glitch-free, high-quality broadcast, enhancing the overall fan experience.

6. Digital Pattern Generators

Digital pattern generators are the unsung heroes in digital system and circuit testing. Unlike their waveform-generating counterparts, these devices produce a sequence of logic levels or digital patterns. 

These patterns are vital for testing the logic and timing of digital circuits, offering a rigorous evaluation of their performance under various conditions.

Typical Applications

  • System-level testing: Validates that complex digital systems function as designed, ensuring inter-component compatibility.
  • IC testing: Useful for assessing individual integrated circuits, identifying any manufacturing defects or design flaws.
  • Debugging: Engineers rely on these generators for troubleshooting problematic circuits, zeroing in on issues related to timing or logic.

Real-World Application
In the automotive industry, digital pattern generators are crucial for ensuring the reliability of electronic control units (ECUs), which govern everything from engine performance to safety systems. 

By simulating various driving conditions using pre-defined digital patterns, engineers can rigorously test the ECUs under diverse scenarios. This helps in identifying any faults or vulnerabilities, thereby ensuring that the vehicle's electronic systems operate flawlessly, even under extreme conditions.

7. Analog Signal Generators

Analog signal generators primarily generate simple continuous wave signals, and they often find applications in older radio and television testing. While they may seem outdated compared to their digital counterparts, they hold significant value for specific tasks. These generators offer metrology-grade frequency and level accuracy, making them essential for high-precision applications.

Real-World Application
In real-world scenarios, analog signal generators play a pivotal role in Doppler radar testing. Their extremely low phase noise characteristics make them ideal for applications that require a high degree of signal purity and stability, such as in radar systems used for weather forecasting and air traffic control.

In these critical setups, any deviation or noise can result in inaccurate data, making the reliable performance of analog signal generators indispensable.

8. Sweep Generators

Sweep generators shine in the area of frequency response testing, particularly in radio frequency (RF) applications. 

Unlike fixed-frequency generators, these devices can automatically vary the output frequency over a specified range, enabling detailed analysis of a system's response to different frequencies.

Typical Applications and Benefits

  • Frequency response testing: Commonly used to measure how devices like amplifiers and filters respond across a range of frequencies.
  • Network analysis: Employed in characterizing the performance of RF networks, helping to optimize signal paths.
  • Benefits over fixed-frequency generators: The ability to sweep through frequencies eliminates the need for manual tuning, saving time and improving accuracy.

Real-World Application
Sweep generators are essential in the medical field, specifically in the development of sophisticated medical devices like MRI machines. These generators help in mapping the frequency response of the machine's RF coils. 

By understanding how the coils respond to different frequencies, engineers can fine-tune the MRI for clearer and more accurate imaging. This ensures both the safety and efficacy of one of the most critical diagnostic tools in modern medicine.

The Value of Used Equipment: Why Every Electrical Engineer Should Consider Refurbished Gear

When you hear "refurbished," you might initially just think "used," but it's crucial to distinguish between the two. 

Refurbished equipment isn't merely second-hand; it has undergone strict quality control, testing, and certification to ensure reliability and performance that meets or even exceeds industry standards.

Top Reasons to Opt for Refurbished Equipment

  • Cost-efficient: Secure high-quality, top-tier equipment without breaking the bank. Refurbished options often cost significantly less than their brand-new counterparts, making advanced technology accessible at a budget-friendly price.
  • Quality guaranteed: Every piece of refurbished equipment undergoes stringent testing and calibration procedures. This meticulous approach ensures the equipment aligns with industry standards, often making it virtually indistinguishable from new gear in terms of performance.
  • Eco-friendly: When you opt for refurbished equipment, you're making an environmentally conscious choice. Reusing hardware reduces the demand for new production, contributing to less e-waste and a smaller carbon footprint.
  • Up-to-date tech: Don't think you're compromising on technology when buying refurbished. Many of these items are relatively new models that come equipped with the latest features, ensuring you stay ahead in the tech game.
  • Reliable warranty: Acquiring refurbished equipment often comes with robust warranties, offering you peace of mind. These warranties frequently rival those of new equipment, giving you added security in your investment.

Refurbished equipment offers not just cost benefits but also assures quality, environmental responsibility, and technological relevance.

What Sets Keysight's Refurbished Equipment Apart?

Keysight sets the gold standard for refurbished equipment, offering an unparalleled blend of quality, reliability, and cost-effectiveness.

Keysight premium used equipment undergoes rigorous refurbishing at the company's largest manufacturing site in Penang, Malaysia. These units are held to the same exacting quality standards as brand-new Keysight products.

Refurbishment Process

  1. Used unit arrives: Each unit first lands at Keysight’s specialized facility in Penang.
  2. Condition check: Immediately after arrival, experts carry out a thorough initial inspection to evaluate the condition of the unit.
  3. Comprehensive cleaning: The equipment undergoes a meticulous cleaning process using vacuum-based technology. Any components that can't be cleaned get replaced.

    Configure & Update
     
  4. Update to latest firmware and software: Once the unit passes its performance checks, it receives updates to the latest compatible firmware and software.
  5. Customization process: Technicians add or remove hardware options, applications, or software options based on customer requirements.
  6. Calibration and safety tests: Rigorous calibration and safety tests ensure that the unit meets or exceeds industry standards.

    Accessories and Final Check
     
  7. Original manuals and accessories: Every refurbished unit comes with the same brand-new accessories and manuals you'd get with a new Keysight instrument.
  8. Final 101-point inspection: Before shipping, the unit undergoes a thorough 101-point quality check, ensuring no detail is overlooked.
  9. Standard like-new warranty: Each factory-refurbished unit benefits from a warranty identical to that of a new Keysight instrument.

    Shipped to Customer
     
  10. Unit packed and shipped to customer: After passing all checks and updates, the unit and its accessories get carefully packed and shipped to the customer.

By choosing Keysight, you're not just getting a piece of equipment; you're investing in peace of mind, backed by a company with a stellar reputation in the industry. The meticulous care put into each refurbished unit translates into a trustworthy and reliable product that can stand up to any challenge.

Important Considerations Before Making a Purchase

Before making a decision on purchasing refurbished equipment, here are some vital points to keep in mind:

  1. Know your needs: Don't just buy equipment because it's available at a great price. Ensure it fits your project requirements both now and in the near future.
  2. Certification matters: Always look for gear that comes with a certification for quality and performance, assuring you of its reliability.
  3. Support and parts: Ensure that the vendor provides robust technical support and has a stock of spare parts for the equipment. This is crucial for minimizing downtime during unexpected maintenance or repairs.

Additional Benefits of KeysightCare
Keysight stands behind the certified quality of their used equipment, offering the KeysightCare package with extended warranty plans for the majority of their refurbished items. Here's why you should consider extending your warranty:

  • Lower costs: Save up to 70% compared to the price of one unplanned repair.
  • Hassle-free process: Skip the administrative troubles; no need for additional purchase orders.
  • Minimal downtime: Enjoy expedited service, reducing delays and resuming your work swiftly.
  • OEM quality: Rest easy knowing you're getting genuine Keysight parts from the people who manufactured the equipment.
  • Global coverage: Transfer your coverage anywhere in the world, giving you flexibility and peace of mind.
  • Predictable expenses: With extended warranties, you can better predict your expenses and safeguard against inflation.

What Else is Included in KeysightCare?
KeysightCare isn't just an extended warranty; it's a full-service package. 

It provides priority response and repair turnaround times, substantially reducing downtime and project delays. 

You get access to a wealth of tech support options, including tutorials, discussion forums, and one-on-one advice from KeysightCare specialists. 

By taking these considerations into account, you're not just making a purchase; you're making a well-informed investment in your work's future success.

Explore Keysight’s Range of Precision Signal Generators On Sale
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
Conclusion: The Power of Choice in Signal Generation

In the intricate realm of electrical engineering, the signal generator you choose can indeed set the tone for excellence.

From waveform generators for basic signal creation to specialized RF vector generators for complex communications testing, understanding the nuances of these indispensable tools is pivotal. 

Each type has its unique features and applications, making the selection process not just a routine purchase but a strategic decision. 

Choose Keysight's meticulously refurbished signal generators for reliability and precision. They are the epitome of quality, guaranteeing that your projects run smoothly and cost-effectively. 

Don't just fill your toolbox, make a choice that ensures sustainability. 

Whenever You’re Ready, Here Are 5 Ways We Can Help You

  1. Browse our premium used network analyzers, oscilloscopes, signal analyzers and waveform generators.
  2. Call tech support US: 1 800 829-4444
    Press #, then 2. Hours: 7am – 5pm MT, Mon– Fri
  3. Talk to our sales support team by clicking the icon (bottom right corner) on every offer page
  4. Create an account to get price alerts and access to exclusive waitlists.
  5. Talk to your account manager about your specific needs.

Great Deals: Function Generators On Sale Right Now