What is Burst Mode?

This article is brought to you by the Keysight Used Equipment Store. The information applies to used and new equipment.

If you know which Keysight model is of interest to you and matches your technical requirements, visit the Used Equipment Store to see if you can save with our offers.
View Our Offers

For more Test and Measurement knowledge and tips, view all technical articles. Visit our resources
Keysight assumes no liability for the completeness, correctness and accuracy of all content on this website and all of its content. Please read here the terms of use of this website.

Your browser limits use of the Used Keysight Equipment website.
Please consider switching to a current version of Chrome, Firefox, Edge or IE11 to use this site.

Did you know that the fastest camera in the world can capture a staggering trillion frames per second? In the realm of oscilloscopes and electrical engineering, we harness a similar principle—albeit not as extreme—using the "Burst Mode". Dive in to uncover the ins and outs of burst mode and its paramount importance in testing electronic systems.

Buy Oscilloscopes at a Great Discount
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
Introduction to Burst Mode

Burst mode in oscilloscopes and related testing equipment refers to a method where a device can generate or capture signals in short sequences or "bursts". These bursts are separated by periods of no activity, allowing the device to handle data at high speeds in short durations, making it invaluable for testing transient and intermittent events.

Key Takeaway
Burst mode in oscilloscopes enables precise and efficient capture of transient and intermittent signals, proving indispensable for modern electrical engineering applications, from digital communications to automotive electronics. Its selective sampling, rapid data processing, and customizable triggering offer unparalleled accuracy and flexibility in testing scenarios.

Understanding the Underlying Principles

Burst mode in oscilloscopes is predicated on capturing or representing signals in defined short bursts. To truly grasp its function and value, we must dissect the primary characteristics that define a burst signal. 

Burst signals possess unique traits that set them apart from continuous signals. Recognizing these traits is vital for electrical engineers aiming to exploit the full capabilities of burst mode.

Duration

Duration denotes the time period over which the burst event transpires. It’s imperative for engineers to understand the duration of a burst as it dictates the window of time they have to capture the signal. The duration can vary greatly, from the exceedingly short bursts in high-speed digital signals to longer pulses in some power electronics applications.

Interval

Interval refers to the time gap that separates successive burst events. A precise knowledge of the interval is crucial as it informs the oscilloscope when the next burst is likely to occur. This is especially relevant for setting up the equipment to be ready to capture or generate the next burst sequence. Some advanced oscilloscopes can adapt in real-time to changing intervals, ensuring consistent data capture even if the signal’s burst behavior is unpredictable.

Amplitude

Amplitude signifies the height or power of the signal, often measured from its baseline or resting state. The amplitude can provide insights into the power or strength of the burst event. For example, in power electronics, a sudden spike in amplitude during a burst could indicate a fault or surge in the system. 

Amplitude can be measured in various units depending on the context—volts for voltage signals, amps for current signals, and so on. 

Oscilloscopes usually provide multiple reference levels to help engineers discern even the minutest changes in amplitude. Modern oscilloscopes, equipped with burst mode, often boast an extensive dynamic range, allowing them to detect both low amplitude bursts (like minor signal perturbations) and high amplitude bursts (like surges or faults) with equal precision.

In essence, understanding these signal characteristics is not just about recognizing their definitions but also about grasping their implications in real-world scenarios. It empowers electrical engineers to harness the power of burst mode, ensuring that transient signals are captured, analyzed, and interpreted with the highest fidelity and accuracy.

Burst Mode in Modern Oscilloscopes

FeatureTraditional OscilloscopesModern Oscilloscopes
SpeedLimited by hardware capabilitiesEnhanced by advanced chipsets and software
Trigger CustomizationBasic trigger conditionsAdvanced triggers with machine learning insights
Data StorageLimited onboard storageExpansive storage with cloud integration
Processing PowerBasic data interpretationAdvanced data analytics and real-time insights

 

Mechanism of Burst Mode

Burst mode in oscilloscopes offers a systematic approach to capturing high-frequency events with surgical precision. The mechanism primarily revolves around three vital steps:

1. Waiting for a Predefined Condition or Trigger

Before any signal capture can begin, the oscilloscope is set in a state of readiness. This primed state ensures the device can detect the exact moment or condition of interest. Users can define what triggers this states, such as:

  • When a signal crosses a specific voltage level (edge trigger)
  • When a pulse has a certain duration (pulse width trigger)
  • When a unique binary pattern appears (pattern trigger)

Modern oscilloscopes offer adjustable trigger sensitivity to ensure the device is neither too responsive, causing false activations, nor too lax, missing crucial signal events.

2. Capturing or Generating a Short Sequence of Data

Once the predefined trigger condition is met, the oscilloscope springs into action, sampling at its maximum rate to capture every detail of the burst event. With the aid of deep memory storage in advanced oscilloscopes, the device can sustain this high-speed sampling throughout the burst without compromising on data integrity. 

At such high sampling rates, maintaining the resolution of the data becomes paramount. For oscilloscopes with multiple channels, the simultaneous capture across all channels ensures the preservation of inter-channel timings and phase relationships.

3. Transitioning to an Idle or “Rest” State

After the high-intensity data capture, the oscilloscope doesn't remain idle. The device's processors might engage in various tasks ranging from signal conditioning to more complex operations, depending on the user's set parameters. The high-resolution data is stored, either in the device's memory or in cloud storage. 

The oscilloscope then re-arms itself, resetting its triggering mechanism to detect the next burst event. Some top-tier models even learn adaptively from previous bursts, refining their settings for future captures. Additionally, by moving to a rest state, the oscilloscope conserves energy and minimizes heat, ensuring longevity.

Burst mode is an embodiment of the delicate balance of anticipation, action, and reflection in modern oscilloscopes. For professionals in the field of electrical engineering, understanding this intricate mechanism equips them to harness the full potential of their oscilloscope, ensuring that every captured event offers insights into their system's transient behaviors.

Key Features and Advantages of Burst Mode

For electrical engineers aiming to achieve precise and insightful test results, comprehending the standout features of burst mode becomes essential. Let's explore these features and the benefits they bring to the table.

Key Features

  • Selective sampling: Unlike continuous sampling, burst mode focuses on capturing data at maximum speeds exclusively during burst events, ensuring no crucial detail is overlooked.
  • Swift data processing: Once a burst is captured, the oscilloscope rapidly processes this data, translating it into usable insights almost instantly.
  • Tailored triggering: One of the shining facets of burst mode is the capacity for engineers to set highly specific trigger conditions, determining precisely when a burst should be initiated.

The Advantages

  • Peak efficiency: Burst mode is the epitome of smart resource utilization. Devices operate at their highest efficiency during burst events, ensuring that they deliver optimal performance without being bogged down during more extended operations.
  • Unparalleled precision: This mode excels in capturing transient and fleeting events with remarkable accuracy. It ensures that even the most intermittent signals are recorded without distortion.
  • Adaptable flexibility: Burst mode isn’t a one-size-fits-all solution. Its design allows for customization, letting engineers tailor settings to match specific test requirements. This ensures data capture is always aligned with the user's needs, eliminating irrelevant noise.

Practical Applications of Burst Mode

Burst mode is not just a feature confined to the technical specifications of oscilloscopes; it has tangible, real-world applications that make a difference in various engineering domains. Let’s delve deeper into some of the sectors where burst mode is proving to be invaluable.

1. Digital Communication Systems

In our digital age, the communication channels are awash with burst data transmissions. As data is often sent in packets or bursts rather than continuous streams, testing and analyzing these intermittent signals becomes critical. Burst mode enables engineers to capture, analyze, and validate the integrity of such data packets, ensuring that modern communication systems, from Wi-Fi networks to satellite links, function reliably and efficiently.

2. Power Electronics

Switching devices in power electronics, such as transistors or IGBTs, frequently exhibit transient responses when they switch on or off. These short-lived events can impact the efficiency and safety of the entire system. With burst mode, engineers can keenly observe these transients, making it possible to fine-tune designs, optimize power conversion, and enhance the reliability of power systems.

3. RF (Radio Frequency) Devices

The world of RF is dominated by waves, and often, these waves are transmitted in short, controlled bursts, especially in modern communication systems. Whether it's a brief signal from a remote sensor or a data burst from a mobile device, burst mode allows for precise measurements of these RF signals. It ensures that devices comply with standards, function optimally, and maintain clarity in communication.

4. Automotive Electronics

Modern vehicles are marvels of electronic integration. From engine control units to infotainment systems, cars today rely on a myriad of electronic components that can exhibit transient behaviors, especially during their start-up or shutdown. 

For instance, the sudden powering on of a car's infotainment system might cause brief signal fluctuations. Burst mode allows engineers to monitor, capture, and analyze these transient events. Such insights are vital for ensuring the longevity, safety, and seamless operation of electronic systems in vehicles.

Conclusion

Burst mode is a true standout, brilliantly blending accuracy, speed, and flexibility. For engineers seeking to capture transient and intermittent signals, understanding and leveraging this mode becomes indispensable. Its ability to offer selective, rapid, and customizable capture makes burst mode an invaluable tool in any electrical engineer's toolkit, aiding in tasks from digital communications to intricate power electronics analyses.

Whether you're a hobbyist looking to delve into this state-of-the-art feature or a professional in need of quality testing equipment, your journey starts at Keysight's Used Equipment Store.

Here quality meets affordability, with an array of used oscilloscopes, network analyzers, signal analyzers and meters, all meticulously inspected and certified by Keysight. It's time to equip yourself with the right tools to tackle modern engineering challenges, and there's no better place to begin than with Keysight's Used Equipment Store.

Browse Oscilloscopes at a Great Discount
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
  1. Browse our Premium Used Oscilloscopes.
  2. Call tech support US: +1 800 829-4444 
    Press #, then 2. Hours: 7 am – 5 pm MT, Mon– Fri
  3. Talk to our sales support team by clicking the icon (bottom right corner) on every offer page
  4. Create an account to get price alerts and access to exclusive waitlists.
  5. Talk to your account manager about your specific needs.

This article is brought to you by the Keysight Used Equipment Store. The information applies to used and new equipment.

If you know which Keysight model is of interest to you and matches your technical requirements, visit the Used Equipment Store to see if you can save with our offers.
View Our Offers

For more Test and Measurement knowledge and tips, view all technical articles. Visit our resources
Keysight assumes no liability for the completeness, correctness and accuracy of all content on this website and all of its content. Please read here the terms of use of this website.