What is a Complementary Metal Oxide Semiconductor (CMOS)?

This article is brought to you by the Keysight Used Equipment Store. The information applies to used and new equipment.

If you know which Keysight model is of interest to you and matches your technical requirements, visit the Used Equipment Store to see if you can save with our offers.
View Our Offers

For more Test and Measurement knowledge and tips, view all technical articles. Visit our resources
Keysight assumes no liability for the completeness, correctness and accuracy of all content on this website and all of its content. Please read here the terms of use of this website.

Your browser limits use of the Used Keysight Equipment website.
Please consider switching to a current version of Chrome, Firefox, Edge or IE11 to use this site.

Did you know that the CMOS technology, which is integral to most of the gadgets we use today, dates back to the 1960s? The Complementary Metal Oxide Semiconductor (CMOS) has seen a remarkable evolution since its inception. 

Today, it's the heart of many electronic devices, from our everyday smartphones to advanced spacecraft systems. As we delve deeper into its intricacies, benefits, and applications, you'll gain a newfound appreciation for this groundbreaking technology and its contribution to our digital age.

Buy Oscilloscopes at a Great Discount
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
Introduction to CMOS

The Complementary Metal Oxide Semiconductor, more commonly known by its acronym CMOS, is a type of semiconductor technology used in myriad electronic devices. At the heart of CMOS technology are two different metal-oxide-semiconductor field-effect transistors (MOSFETs) – the PMOS and NMOS transistors. Working together, they form the foundation for digital integrated circuits.

Key Takeaway
Complementary Metal Oxide Semiconductor (CMOS) technology stands as an architectural pillar in the current age of electronics. Its profound impact spans across various applications, ranging from digital logic circuits and imaging sensors to analog circuits and integrated SoCs (System on Chips). What distinguishes CMOS is its inherent efficiency, low power consumption, high noise immunity, versatility, and scalability.

How CMOS Technology Works

To understand the function and benefits of CMOS, it's imperative to delve deeper into its building blocks.

N-type and P-type MOSFETs

MOSFETs can be either N-type or P-type:

  • N-type (NMOS) transistor: Comprises a negative charge (electron) carrier. It turns on or becomes conductive when a positive voltage is applied.
  • P-type (PMOS) transistor: Utilizes a positive charge (hole) carrier. It turns on when a negative voltage is applied.

The Complementary Nature

The 'complementary' in CMOS stems from the use of both NMOS and PMOS transistors. In digital circuits:

  • When the NMOS transistor is on (or active), the PMOS is off (or inactive).
  • Conversely, when the PMOS is on, the NMOS is off.

This complementary operation ensures that at any given time, only one type of transistor is conducting. This feature greatly reduces power consumption, especially when the circuit is in a static or standby state.

Advantages of CMOS

CMOS technology is widely used in electronics because of its many advantages. While the technology has several advantages, four of them stand out as particularly defining.

Low Power Consumption

The inherent design of CMOS circuits, where only one type of transistor (either NMOS or PMOS) conducts at any given time, is the key behind its power efficiency. Let's delve deeper:

  • Idle efficiency: In many digital circuits, there are moments when the circuit isn't switching and remains in a static state. During these moments, CMOS circuits consume negligible power due to the absence of a direct current path between the power supply and ground.
  • Heat production: Devices that consume less power inherently produce less heat. This means that devices employing CMOS circuits tend to have longer lifespans and require less cooling.
  • Battery life: For portable devices, power efficiency translates to extended battery life. With the increasing demand for mobile gadgets, the low power consumption of CMOS makes it an obvious choice for designers.

High Noise Immunity

In the world of electronics, noise can be a major hindrance to performance. CMOS's resilience against noise sets it apart.

  • Threshold tolerance: CMOS circuits have distinct voltage thresholds for logic '0' and logic '1'. This ensures that minor fluctuations, due to noise, do not inadvertently change the state of a circuit.
  • Stable outputs: The high noise immunity ensures that CMOS outputs remain stable even in less-than-ideal conditions, making them reliable for critical applications.
  • Consistent performance: Whether it's in a pristine lab environment or a cluttered workspace with multiple devices, CMOS circuits consistently perform, unaffected by the surrounding electrical noise.

Versatility

The versatility of CMOS circuits is a boon for designers:

  • Wide operating voltage range: CMOS devices can function over a wide range of power supply voltages, making them suitable for varied applications—from tiny wearables to large industrial machines.
  • Mixed signal applications: CMOS can be combined with other technologies, enabling the creation of mixed-signal chips (combining digital and analog functions), which are vital in applications like RF communications.
  • Design flexibility: The ability to function under different conditions means designers have more freedom, allowing for greater innovation and customization.

Scalability

One of the pivotal advantages of CMOS is its scalability.

Moore's Law in action: Over the years, the dimensions of CMOS transistors have reduced significantly, often in line with Moore's Law. This has enabled the integration of billions of transistors on a single chip.

Performance gains: As transistor dimensions shrink, the switching speed often increases. This results in faster chips without a proportional increase in power consumption.

Cost-effective production: Smaller transistors mean more chips per wafer and a lower cost per function, making devices more affordable to the end consumer.

CMOS vs. Bipolar Junction Transistor (BJT) Technology

Here's a brief table to compare CMOS with its predecessor, the BJT.

ParameterCMOSBJT
Power ConsumptionVery Low (especially in idle state)Higher, constant current flow
SpeedModerate, improves with scalingTypically faster
Integration DensityHigh, suitable for large-scale integration (LSI)Lower
Noise ImmunityHighModerate
Voltage Supply RangeWideNarrower

 

Applications of CMOS Technology

The expansive reach of CMOS technology is evident in numerous facets of modern electronics.

Digital Logic Circuits

Digital logic circuits form the cornerstone of digital systems, and CMOS is instrumental in their architecture. Computer processors, the heart of every computing device, use CMOS-based logic gates to handle vast computational tasks at lightning speeds. 

This is paralleled by memory chips like RAM (Random Access Memory) and flash storage that bank on CMOS for their efficiency. The very foundation of these systems, the basic logic gates such as AND, OR, and NOT, are built using CMOS transistors.

Imaging Sensors

In the domain of imaging sensors, CMOS has significantly reshaped our image capturing and processing capabilities. Digital cameras have seen a shift in the adoption of the CMOS image sensor, which effectively converts light into electrons. This change is driven by the sensor's ability to amalgamate a plethora of functionalities, offering flexibility while trimming down costs. 

Notably, the ubiquitous smartphone cameras, which demand superior image quality in compact form factors, extensively utilize CMOS sensors. This ensures that even during extended photography sessions, the device's battery remains optimally used.

Analog Circuits

When we consider analog circuits, CMOS, despite being renowned for digital applications, showcases its versatility. Data converters, especially Analog-to-Digital Converters (ADCs) and Digital-to-Analog Converters (DACs), serve as bridges between analog and digital realms. Their efficient and swift operations are largely attributed to CMOS. 

With the surge in integrated wireless communication systems, CMOS-based Radio Frequency (RF) circuits have become the norm. Even amplifiers, including operational amplifiers (op-amps), are gravitating towards CMOS technology, leveraging its wide bandwidth and power efficacy.

SoCs (System on Chips)

Lastly, the advent of SoCs (System on Chips) is a testament to the advances in electronics, aiming to bundle multifarious functionalities into a singular compact unit. These chips, integrating components ranging from processors and memory to RF modules, exemplify streamlined design. Mobile devices, particularly smartphones and tablets, heavily rely on SoCs. Their ability to conserve energy, courtesy of CMOS, ensures longer device runtimes.

Beyond just mobile devices, specialized systems encompassing sectors from automotive electronics to smart home appliances employ SoCs, with CMOS being a central component.

CMOS in Oscilloscopes and Testing Equipment

For electrical engineers and those in related fields, the role of CMOS is paramount in the realm of oscilloscopes and testing equipment.

  1. High-speed oscilloscopes: With the scalability of CMOS, oscilloscopes can now probe faster signals with higher accuracy.
  2. Analog-to-Digital Converters (ADCs): CMOS technology aids in faster and more energy-efficient ADCs, crucial in digital storage oscilloscopes.
  3. Portable testing equipment: Due to low power consumption, CMOS finds its place in battery-operated testing devices, prolonging battery life.

Conclusion

The journey through the realm of Complementary Metal Oxide Semiconductor (CMOS) technology underscores its many benefits that have been instrumental in shaping the modern electronic landscape. With unparalleled energy efficiency, scalability, high noise immunity, and versatility, CMOS proves to be a cornerstone in the progress and innovation of digital and analog systems alike. 

As we stand at the cusp of rapid technological advancement, tools that aid in designing, testing, and validating these CMOS-based systems become paramount.

For professionals keen on diving deeper into the exploration and testing of CMOS applications, Keysight's Used Equipment Store is for you. Not only does it offer an array of premium equipment like oscilloscopes, network analyzers and meters, but it also ensures cost-effective solutions for both budding and seasoned engineers. 

Dive into the future of electronics with Keysight's trusted tools by your side.

Browse Oscilloscopes at a Great Discount
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
  1. Browse our Premium Used Oscilloscopes.
  2. Call tech support US: +1 800 829-4444 
    Press #, then 2. Hours: 7 am – 5 pm MT, Mon– Fri
  3. Talk to our sales support team by clicking the icon (bottom right corner) on every offer page
  4. Create an account to get price alerts and access to exclusive waitlists.
  5. Talk to your account manager about your specific needs.

This article is brought to you by the Keysight Used Equipment Store. The information applies to used and new equipment.

If you know which Keysight model is of interest to you and matches your technical requirements, visit the Used Equipment Store to see if you can save with our offers.
View Our Offers

For more Test and Measurement knowledge and tips, view all technical articles. Visit our resources
Keysight assumes no liability for the completeness, correctness and accuracy of all content on this website and all of its content. Please read here the terms of use of this website.