Mastering Power Device Testing: A Guide to Electronic Loads

This article is brought to you by the Keysight Used Equipment Store. The information applies to used and new equipment.

If you know which Keysight model is of interest to you and matches your technical requirements, visit the Used Equipment Store to see if you can save with our offers.
View Our Offers

For more Test and Measurement knowledge and tips, view all technical articles. Visit our resources
Keysight assumes no liability for the completeness, correctness and accuracy of all content on this website and all of its content. Please read here the terms of use of this website.

Your browser limits use of the Used Keysight Equipment website.
Please consider switching to a current version of Chrome, Firefox, Edge or IE11 to use this site.

In a world where power is the lifeblood of technology, you and other engineers are constantly seeking ways to optimize and validate the performance of various power sources. 

Balancing stability and efficiency across countless load conditions is no small feat, and navigating this challenge can be daunting. 

The solution lies in electronic loads that empowers you to push the boundaries of power devices, testing and simulating real-world conditions with unparalleled precision. 

This article will look at the intricacies of electronic loads, exploring direct current (DC) electronic loads, load types, and transistor/FET concepts.

Understanding how these essential tools work is the key to revolutionizing the engineering world, enabling you to unlock the full potential of your power sources.

What Are Electronic Loads?

Imagine a device that can sink and absorb power from a power source. Electronic loads are designed to do just that, allowing you to accurately test and measure the voltage, current, and power characteristics of various devices under various load conditions. 

These loads provide real-time feedback on the performance of your energy source equipment, enabling you to make adjustments or corrections quickly and easily.

Key Takeaway
Electronic loads are test instruments that mimic real-world loads to test the performance of power devices, such as power supplies and batteries.

Find Oscilloscopes for With Huge Discounts
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
DC Electronic Load

A DC electronic load is an instrument designed to assess the performance of Direct Current power sources by drawing a specific load current. 

It provides a wide range of operating modes, including

  1. Constant Current (CC) Operation
  2. Constant Voltage (CV) Operation
  3. Constant Resistance (CR) Operation
  4. Constant Power (CP) Operation

These modes enable engineers to test power sources under various load conditions, ensuring their devices meet the required performance standards.

In addition to these operating modes, electronic loads are also designed with safety features such as overvoltage and overcurrent protection. This ensures that the load and power source remain undamaged during testing, allowing you to safely explore the device's capabilities.

Whether you're testing batteries, power supplies, solar panels, or any other DC-powered device, electronic loads are the perfect companion for validating power source performance.

Constant Current (CC) Operation

In constant current mode, the electronic load maintains a constant current regardless of changes in the input voltage. This mode is essential for testing power sources such as batteries, fuel cells, and solar panels, where the load current is a critical parameter. 

It also helps assess the power supply's current protection and conservation capabilities, ensuring the device remains safe and does not dissipate more power than necessary.

The key benefits of CC operation are

  • It can provide a simulation of a wide range of current loads and simulate peak loading conditions.
  • It allows for precise control over the load current, enabling you to assess a device's performance under various operating conditions.
  • It enables you to quickly identify any issues with the power source and make adjustments as needed.

CC operation can test power sources under light and heavy load conditions, ensuring the device meets the required performance standards.

It is essential for validating battery lifetime and evaluating a product's design capabilities. For instance, it can help identify issues with the power source's regulation circuitry. Then, you can optimize your design for maximum efficiency and performance.

Constant Voltage (CV) Operation

The constant voltage mode allows the electronic load to maintain a stable output voltage, regardless of fluctuations in load current. This mode is crucial for testing power supplies and uninterruptible power supplies (UPS), ensuring they can provide a stable voltage under varying load conditions.

It also enables power supply testing for power factors and output power, which is essential for validating power device performance. 

The key benefits of CV operation are

  • It allows you to simulate various voltage loads and peak loading conditions, allowing for accurate testing.
  • It enables precise control over the load voltage.
  • It provides real-time feedback on the performance of the power source, allowing you to identify any issues and make adjustments quickly as needed.

You will find examples of CV operations in automotive, industrial, and consumer applications. For instance, it can test automotive power supplies, industrial uninterruptible power supplies, and consumer power adapters.
 

Constant Resistance (CR) Operation

In constant resistance operation, the electronic load emulates a resistive load by maintaining a constant ratio between the voltage and current. This mode is vital for testing power devices with a defined source resistance, such as power electronic circuits and switching devices. 

Some real-life examples of CR operation include LED drivers, motor controllers, and electronic transformers. CR operations also test power electronics such as DC-DC converters, which require a constant resistance to evaluate the output voltage stability.

The advantages of the CR mode are

  • It provides a precise load resistance to assess device performance accurately.
  • It allows you to simulate various resistive conditions, enabling peak loading testing.
  • It enables quick and easy troubleshooting, helping identify power source issues.

Constant Power (CP) Operation

Constant power operation enables the electronic load to maintain constant load power regardless of input voltage or current changes. This mode is helpful for testing power supplies and regenerative power supplies, where power consumption and average power ratings are essential parameters.

In consumer electronics, CP operations are used to test devices such as battery chargers and AC adapters. It is also widely used in automotive applications, where it helps evaluate a vehicle's power management system.

The primary benefits of CP operation include

  • Assessment of power consumption and average power ratings for power supplies and regenerative power supplies.
  • Simulation of dynamic load conditions, allowing you to accurately assess device performance under peak loading conditions.
  • Real-time feedback on device performance.

Types of Loads

In the world of electronics testing, loads are like tools—you need the right tool for the job. Here are some of the most common types of loads

  1. Capacitive Load
  2. Inductive Load
  3. Resistive Load

Understanding the type of load and selecting the right tool for your application will help ensure accurate, reliable testing results. Let's take a look at each.

Capacitive Load

A capacitive load consists of capacitors and electronic components that store electrical energy temporarily. These loads can influence the power supply's voltage sources, as they tend to draw large amounts of current when the supply voltage changes rapidly.

The primary characteristics of capacitive loads are

  1. They draw large amounts of current when the supply voltage changes rapidly.
  2. They are used to test power supplies and other devices that must be able to handle sudden load changes.
  3. They can measure parameters such as frequency and average current.

Capacitive loads are commonly used in automotive testing and industrial and consumer applications.

Inductive Load

Inductive loads consist of coils or inductors that store energy in a magnetic field. They can affect the power supply's current source, as the current changes within the coils cause voltage spikes and require protection circuitry.

The characteristics of inductive loads include

  • Energy storage in magnetic fields.
  • Potential for voltage spikes due to current changes within coils.
  • Requirement for protection circuitry.

Inductive loads are used in various applications, including power electronics and motor testing. Since inductive loads can cause voltage spikes, they require additional protection circuitry to ensure stable operation.

Resistive Load

Resistive loads are the most common type of load, consisting of resistors that dissipate power as heat. They can simulate real loads, such as electronic devices and mains power applications, providing a straightforward means of testing power circuit performance.

In real-world applications, resistive loads are commonly used to

  1. Test power supplies
  2. Evaluate the performance of electronic devices
  3. Simulate mains power applications

Resistive loads offer the flexibility to vary resistance levels and simulate various conditions, enabling accurate peak loading tests. This ability makes them ideal for troubleshooting, diagnostics, and power circuit design.

Transistors (FET)

A transistor, or Field-Effect Transistor (FET), is a semiconductor device that amplifies or switches electronic signals and power in electronic circuits. They are essential components in various power devices, including power supplies and management systems.

They have many benefits, including

  1. Low power consumption
  2. Small in size
  3. High switching speed
  4. High-frequency operation
  5. Compatibility with other components

FETs are used in various consumer electronics applications. They are used as switches or amplifiers and are essential for power circuits. Understanding the characteristics of FETs is vital in designing efficient and reliable power systems.

Understanding RDS Values

RDS (Resistance Drain-to-Source) is the resistance between the drain and source terminals of a FET when it is fully conducting. A low RDS value indicates a more efficient FET with reduced power consumption, crucial for power conservation and power factors in power devices.

Low RDS values also reduce the risk of thermal runaway and ensure the reliable operation of power devices. FETs with lower RDS values can also be used at higher current levels without risking excessive heating or damage.

RDS is an important parameter to consider when designing power electronics, as it can affect the efficiency of a device. 

What Is a Slew Rate?

The Slew Rate is the rate at which the output voltage of an electronic device, such as a transistor or FET, can change over time in response to a change in the input signal. It is typically expressed in volts per microsecond (V/µs) and is a critical parameter for determining the performance of power-switching devices and electronic circuits. 

A higher slew rate indicates that the device can respond more quickly to changes in the input signal, enabling efficient and accurate power management in dynamic load conditions.

A low slew rate indicates that the device will lag in responding to changes, leading to poor performance and unreliable operation. So, it is important to consider the slew rate when selecting power-switching devices for power electronics applications, as it can influence system performance.

Summary

Electronic loads play a crucial role in the engineering world, providing you with the means to test and validate the performance of power sources effectively. Understanding the different operating modes, load types, and transistor/FET concepts allows you to optimize your power devices and ensure reliable, efficient operation in real-world conditions.

Keysight Oscilloscopes

Buying a used oscilloscope is the best way to save money without sacrificing quality. You can save up to 90% when purchasing from Keysight Technologies!

We provide many options – from basic oscilloscopes to premium models backed by a 1-year warranty. With Keysight, you can be confident you are choosing a quality oscilloscope supported by a trusted manufacturer.

Browse Oscilloscopes for Sale
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
This article is brought to you by the Keysight Used Equipment Store. The information applies to used and new equipment.

If you know which Keysight model is of interest to you and matches your technical requirements, visit the Used Equipment Store to see if you can save with our offers.
View Our Offers

For more Test and Measurement knowledge and tips, view all technical articles. Visit our resources
Keysight assumes no liability for the completeness, correctness and accuracy of all content on this website and all of its content. Please read here the terms of use of this website.