Types of Oscilloscope: Discovering the Best Option for Your Needs

Your browser limits use of the Used Keysight Equipment website.
Please consider switching to a current version of Chrome, Firefox, Edge or IE11 to use this site.

Did you know that the first true oscilloscope, created in the early 20th century, was a simple device relying on a cathode-ray tube to visually represent signal voltages? Fast-forward to today, and we're using oscilloscopes that can not only capture fleeting electrical signals but also analyze them in depth with digital precision. 

If you're an engineer, this step from analog to digital is more than just technological advancement; it governs how you approach diagnostics and design in the electronic world. 

But with this impressive evolution, comes a crucial question: How do you know which oscilloscope is the best fit for your specific needs in this vast sea of options? 

This guide is here to help you navigate through the features, types, and capabilities to find the perfect oscilloscope for your engineering needs. Ready to find your match?

Types of Oscilloscopes

TypeDisplaySignal AnalysisPortabilityBest Used For
Analog OscilloscopesAnalog CRTReal-timeBulky, stationaryBasic waveform observation
Digital Storage OscilloscopesDigitalDeep memory, complex analysisVariable sizesGeneral purpose, detailed analysis
Digital Phosphor OscilloscopesDigital with PhosphorFast waveform capture rateSimilar to DSOsDynamic signals, high-frequency
Mixed-Signal OscilloscopesDigitalAnalog + Digital signalsVariable, often compactCircuits with analog and digital components
Mixed Domain OscilloscopeDigitalFrequency + Time domainVariable, often largerTime and frequency domain analysis
Digital Sampling OscilloscopesDigitalHigh-speed, under-samplingCompactHigh-speed digital signals
Handheld OscilloscopesDigital or AnalogPortable, real-timeHighly portableField service, simple diagnostics
PC-Based OscilloscopesComputer ScreenFlexible, requires PCDepends on PCCustom applications, research
USB OscilloscopesComputer ScreenFlexible, requires PCHighly portableMobile diagnostics, education
Automotive OscilloscopesDigitalSpecialized for automotiveDesigned for field useAutomotive diagnostics, troubleshooting

Elevate Your Engineering with Keysight Certified Refurbished Oscilloscopes
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
1 – Analog Oscilloscopes

Analog oscilloscopes operate on a simple principle. They directly display an electrical signal by deflecting an electron beam across a cathode-ray tube (CRT), painting a picture of voltage over time. This direct, real-time visualization allows for an intuitive understanding of signal characteristics such as amplitude, frequency, and noise.
Historically, analog oscilloscopes were the first window into the invisible world of electronic signals. They laid the foundation for modern electronics diagnostics, enabling groundbreaking discoveries and innovations. 
Even today, in a niche of applications, analog oscilloscopes are preferred for their unparalleled real-time response and analog warmth. They shine in educational settings, where understanding fundamental electronics principles is key, and in troubleshooting older technology, where the subtleties of analog signals are essential.

Pros:

  • Immediate signal display without delay, perfect for real-time monitoring.
  • Simple and intuitive operation, ideal for educational purposes.
  • Excellent at displaying signal variations and anomalies in real time.

Cons:

  • Limited in features and measurement accuracy compared to digital models.
  • Bulky and heavy due to CRT technology.
  • Lacks storage, analysis, and digital signal processing capabilities.

Despite their limitations in today's digital age, analog oscilloscopes still hold a place in areas where the feel of analog is irreplaceable, offering a tactile connection to the fundamentals of electronic signals.

2 – Digital Storage Oscilloscopes (DSO)

Digital Storage Oscilloscopes (DSOs) have completely transformed the way we perceive, capture, and analyze electronic signals.  Unlike their analog counterparts, DSOs convert incoming signals into digital format using an analog-to-digital converter (ADC). This allows for the storage of waveforms in memory, enabling detailed analysis and comparison of signals over time. 
DSOs marked a significant shift in oscilloscope technology, offering features like waveform storage, pre-trigger viewing, and extensive signal analysis capabilities.
Key features of DSOs include their ability to capture rare or transient events, deep memory for storing long waveforms, advanced analysis tools (such as FFT for frequency analysis), and digital connectivity options for data sharing and remote control. 
These features make them valuable in a wide range of applications, from research and development to repair and maintenance, and even in educational settings for teaching complex electronic concepts.

Benefits of DSOs:

  • Precision and versatility: High sampling rates and deep memory allow for precise measurement and analysis of complex signals.
  • Storage and analysis: Ability to store and analyze waveforms digitally, allowing post-capture processing and comparison.
  • User-friendly: Many DSOs come with intuitive interfaces, easy navigation, and touchscreens, making complex analyses more accessible.

DSOs are suited for various applications, offering flexibility that analog oscilloscopes can't match. They're used in designing and testing new electronic devices, troubleshooting and repairing circuits, conducting scientific research, and in education to demonstrate electronic principles. 
Their range of functionalities—from simple signal checking to complex data analysis and automated measurements—makes them indispensable tools in modern electronics labs.

3 – Digital Phosphor Oscilloscopes (DPO)

Digital Phosphor Oscilloscopes (DPOs) take the digital oscilloscope's capabilities a step further. They offer advanced visualization techniques that mimic the look and feel of analog oscilloscopes while providing the benefits of digital technology. 
DPOs use a parallel processing architecture to capture, display, and analyze signals in real-time, offering a more dynamic view of signal activity compared to DSOs.
The key to their superior visualization lies in their ability to display signal intensity, which helps engineers and technicians to easily identify rare or transient events and understand signal patterns over time. 
This intensity grading, reminiscent of the glow of phosphor on analog oscilloscopes, gives a more nuanced view of waveform behavior, making it easier to spot anomalies like jitter, glitches, or temporary faults.

Compared to DSOs, DPOs provide:

  • Faster waveform update rates, resulting in a smoother, more detailed display of signal variations.
  • Intensity-graded displays that highlight the frequency of occurrence of signal events, offering deeper insights into signal behavior.

DPOs are particularly valued in fields requiring detailed signal analysis and troubleshooting under dynamic conditions, such as telecommunications, automotive electronics, and radar system development. 
In these scenarios, the ability to quickly identify and analyze signal anomalies is crucial, making DPOs the preferred choice for engineers looking for depth and detail in their signal analysis toolkit.

    4 – Mixed-Signal Oscilloscopes (MSO)

    Mixed-Signal Oscilloscopes (MSOs) are a hybrid between traditional oscilloscopes and logic analyzers, uniquely designed to analyze and display both analog and digital signals simultaneously. This dual capability allows engineers to observe and correlate the behavior of mixed-signal circuits in real-time, providing a comprehensive view of a system's performance. 

    MSOs are equipped with analog channels, for observing waveforms, and digital channels, for monitoring logic signals, making them indispensable in today’s complex electronic environments.

    The primary advantage of using an MSO is its ability to give engineers a clear view of a mixed-signal system. This is crucial in applications where analog signals interact closely with digital components, such as in embedded systems, where timing between various elements can significantly affect performance. 

    By displaying analog and digital signals side by side, MSOs allow for precise timing analysis, signal integrity checks, and debugging at both the signal and system levels.

    Applications where MSOs prove invaluable include:

    • Embedded system design and debugging: MSOs can track down issues in communication between microcontrollers and analog inputs/outputs.
    • Automotive electronics: With vehicles increasingly relying on mixed-signal systems, MSOs are used to diagnose issues in sensor data processing and network communications.
    • Consumer electronics: MSOs help in designing and troubleshooting devices that combine analog audio signals with digital controls, ensuring seamless integration.

    In these and other scenarios, MSOs provide critical insights by allowing engineers to see the interaction between analog waveforms and digital logic, insights that might be challenging or impossible to obtain with either a purely digital or analog oscilloscope.

    5 – Mixed Domain Oscilloscope (MDO)

    Mixed Domain Oscilloscopes (MDOs) push the boundaries of traditional oscilloscope capabilities by not only offering mixed-signal analysis (combining analog and digital channels) but also integrating RF (radio frequency) analysis
    This comprehensive approach allows engineers to tackle the complexities of modern wireless communications, IoT devices, and other RF-intensive applications within a single instrument, spanning time, frequency, and modulation domains.
    MDOs are invaluable in the realm of wireless communications, where dissecting the interplay between RF and digital signals can uncover critical insights into device performance and reliability. In the rapidly evolving IoT sector, MDOs ensure devices communicate effectively, free from RF interference, which is key to operational success.

    The standout benefits of MDOs include:

    • Comprehensive analysis: Seamlessly integrates spectrum analyzer, oscilloscope, and logic analyzer functions to provide a full spectrum of analysis in time, frequency, and modulation domains.
    • Streamlined workflow: Reduces the need for multiple specialized instruments, saving on cost and bench space while simplifying the testing setup.

    By providing a single perspective on a device's functions across various areas, MDOs streamline the design and testing process and open new avenues for innovation in wireless technology development and RF signal integrity troubleshooting.

    6 – Digital Sampling Oscilloscopes

    Digital Sampling Oscilloscopes (DSOs) operate on a principle that allows them to analyze signals that are much higher in frequency than the oscilloscope's own bandwidth would typically permit. This is achieved through the use of equivalent time sampling (ETS), a method where the oscilloscope samples the high-frequency signal at several points over multiple cycles, effectively building a complete waveform over time. 
    This technique makes them especially adept at capturing and analyzing very high-frequency signals, often up to the gigahertz range, which are beyond the reach of conventional real-time oscilloscopes.
    The unique ability of digital sampling oscilloscopes to handle such high frequencies makes them indispensable in specific applications where precision and detail in the high-frequency domain are crucial. These include:

    • Telecommunications: For analyzing the integrity of high-speed serial data streams, such as those used in fiber optic and Ethernet communications.
    • Radar systems: For capturing and evaluating the fast, pulsed signals used in radar, where accurate timing and waveform shape are critical for system performance.
    • Semiconductor testing: For measuring the performance of high-speed digital circuits, where understanding the exact shape and timing of signals is necessary to ensure reliability and functionality.

    Digital sampling oscilloscopes offer capabilities that other types of oscilloscopes simply cannot, providing essential insights into the behavior of high-frequency signals and ensuring the performance and integrity of advanced electronic systems.

    7 – Handheld Oscilloscopes

    Handheld oscilloscopes are the epitome of convenience and portability in electronic diagnostics. Designed for on-the-go use, these compact devices are usually battery-operated, allowing engineers and technicians to conduct measurements and analysis directly in the field, without the need for an external power source. Their rugged design and ease of use make them well-suited for challenging environments where portability is essential.

    While handheld oscilloscopes offer unparalleled portability, this advantage comes with certain trade-offs. Handheld models may have limited bandwidth, fewer channels, and less advanced analysis features compared to their benchtop counterparts. The display size and resolution might also be smaller, which could make waveform analysis more difficult. However, for many applications, these trade-offs are well worth the benefits of mobility and accessibility.

    Potential use cases for handheld oscilloscopes include:

    • Field service and maintenance: Ideal for troubleshooting and repairing equipment in industrial, telecommunications, and utility settings.
    • On-the-go diagnostics: Handy for service technicians and engineers needing to make quick, on-site diagnostics or check electronic components in remote locations.
    • Education and training: Useful for teaching environments where mobility allows for a more interactive and practical learning experience.

    Handheld oscilloscopes strike a balance between functionality and convenience, providing essential diagnostic capabilities directly at the point of need, whether in the field, on the factory floor, or in remote locations.

    8 – PC-Based Oscilloscopes

    PC-based oscilloscopes transform the way we approach electronic measurements by leveraging the processing power and display capabilities of a computer. 

    These oscilloscopes consist of a hardware interface that captures the signal, which is then sent to a computer where specialized software processes, displays, and analyzes the data

    This reliance on a computer for the heavy lifting allows these oscilloscopes to be highly flexible and customizable, adapting to a wide range of applications and user needs.

    The advantages of PC-based oscilloscopes are significant:

    • Software flexibility: The software can be updated or customized, offering tailored analysis features and user interfaces.
    • Upgradability: As software can be easily updated, the oscilloscope can benefit from new features and improvements without needing to replace the hardware.
    • Cost savings: Without the need for a built-in display or processing unit, PC-based oscilloscopes can be more cost-effective, especially for users who already have a compatible computer.

    Suitable applications for PC-based oscilloscopes include:

    • Education: Their flexibility and cost-effectiveness make them ideal for teaching environments, where they can be used to demonstrate a wide range of electronic principles and experiments.
    • Small-scale projects and hobbyists: DIY enthusiasts and small-scale developers can benefit from the adaptability and affordability of PC-based oscilloscopes, making advanced electronic analysis accessible without a significant investment.

    PC-based oscilloscopes offer a compelling mix of versatility, upgradability, and value, making them especially suited for settings where innovation, education, and budget are key considerations.

    9 – USB Oscilloscopes

    USB oscilloscopes embody the essence of portability and simplicity in the world of electronic diagnostics. These devices connect directly to a PC via a USB port, transforming the computer into a powerful oscilloscope with the help of specialized software. 

    The compact size and USB connectivity make these oscilloscopes exceptionally easy to set up and use, offering a convenient solution for users who need to perform electronic measurements without the bulk or expense of traditional benchtop models.

    Benefits of USB oscilloscopes include:

    • Ease of setup: Simply plug the device into a PC, install the software, and it's ready to use.
    • Portability: Their small size and reliance on a laptop or desktop for processing and display make them ideal for fieldwork or any situation where mobility is a priority.
    • Cost-effectiveness: USB oscilloscopes are generally more affordable than their standalone counterparts, making them accessible to a wider range of users.

    However, these advantages come with certain limitations:

    • Performance might not match that of more sophisticated oscilloscopes, with potential constraints in bandwidth, sampling rate, and analysis features.
    • Dependence on a computer means that if the PC has issues, it could affect the oscilloscope's functionality.

    Typical users and scenarios for USB oscilloscopes include:

    • Students and educators: For learning and teaching electronics, where ease of use and cost are critical.
    • Hobbyists and DIY enthusiasts: For home projects where space and budget are limited.
    • Field technicians: Who require a lightweight, portable solution for troubleshooting and diagnostics on the go.

    USB oscilloscopes strike a balance between functionality and convenience, making them a suitable choice for users who prioritize ease of use, portability, and affordability in their electronic measurement tasks.

      10 – Automotive Oscilloscopes

      Automotive oscilloscopes are specialized tools designed specifically for vehicle diagnostics and troubleshooting. They are equipped with features tailored to the needs of automotive technicians and hobbyists, making them indispensable for working on vehicle electronics.

      Specialized features of automotive oscilloscopes include:

      • Higher voltage ranges: To accommodate the higher voltages present in automotive systems.
      • Pre-set test routines: For common automotive tests, such as injector waveforms, ignition systems, and starter motors.
      • Robust build: Designed to withstand the harsh environments of automotive work.

      These oscilloscopes excel in performing specific automotive-related measurements and tests, such as:

      • Engine performance analysis: Monitoring sensor data and ignition signals to diagnose engine issues.
      • Electrical system checks: Assessing battery health, alternator output, and identifying parasitic drains.
      • CAN bus and other network diagnostics: Analyzing data transmission issues in vehicle communication networks.

      The value they bring to automotive technicians lies in their ability to:

      • Diagnose complex issues quickly: Providing real-time data and analysis to pinpoint problems in modern vehicle electronics.
      • Improve repair accuracy: By allowing for precise measurement of electrical signals, technicians can make informed repair decisions.
      • Save time and money: Reducing diagnostic time and avoiding unnecessary parts replacement.

      Automotive oscilloscopes are essential tools for anyone involved in vehicle maintenance and repair, offering detailed insights into the complex electronic systems that control modern vehicles.

      Applications and Uses of Oscilloscopes

      Oscilloscopes, with their diverse functionalities, are indispensable across various industries, demonstrating their wide-ranging applications.

      • Education: Oscilloscopes, ranging from basic analog to more sophisticated digital storage models, are foundational in teaching the principles of electronics, allowing students to visualize and understand electronic signals and behaviors.
      • Research: High-end oscilloscopes like digital phosphor oscilloscopes and mixed domain oscilloscopes are indispensable in research settings. They provide the precision and flexibility needed for groundbreaking experiments, capturing detailed signal anomalies and facilitating the integration of disparate signal types.
      • Engineering: The development and testing of electronic systems heavily rely on mixed-signal oscilloscopes, which offer the unique ability to analyze both analog and digital signals, crucial for the design of integrated circuits and systems.
      • Automotive diagnostics: Specialized automotive oscilloscopes are tailored for the automotive industry, enabling technicians to diagnose and troubleshoot the complex electronic systems that control modern vehicles, from engine management to sensor networks.

      Through these examples, it becomes evident that oscilloscopes serve as more than just measurement tools; they are integral to the advancement, education, and maintenance within tech-centric industries. Each type of oscilloscope brings specific capabilities to the table, ensuring that professionals across disciplines have the precise tools they need to tackle their unique challenges.

      5 Steps to Choosing the Right Oscilloscope for Your Project

      Choosing the right oscilloscope for your project is crucial to ensuring accurate data collection and analysis. Whether you're working in electrical manufacturing, aerospace, or any field that relies on electronic measurements, understanding your project requirements is key. 

      Here are 5 steps to follow to help you make an informed decision.

      1. Bandwidth and Sample Rate Requirements

      Bandwidth and sample rate are critical to capturing accurate signal representations. Bandwidth determines the range of frequencies the oscilloscope can accurately measure, while the sample rate affects the detail with which it can capture rapid changes in the signal. For high-speed applications like aerospace, look for a scope with a high bandwidth and sample rate to match the fastest signal component you need to measure.

      2. Number of Channels Needed

      The number of channels determines how many signals you can observe simultaneously. More channels allow for more complex system diagnostics, especially useful in fields like electrical manufacturing where observing the interaction between multiple signals is often necessary.

      3. Specific Features for Your Application

      Consider specific features that could enhance your project's efficiency. Advanced analysis options, deep memory depth, and connectivity options (such as USB or Ethernet) can be vital for complex applications. For example, aerospace projects might benefit from advanced analysis features to decode serial buses or perform spectral analysis.

      4. Portability and Form Factor

      The work environment greatly influences the choice between benchtop, handheld, or portable oscilloscopes. Handheld models offer flexibility for fieldwork, while benchtop oscilloscopes provide more comprehensive features and higher performance for lab settings. Consider where and how you'll use the oscilloscope most frequently.

      5. Budget and Cost-Effectiveness

      Finally, balance your budget with your needs. While it's tempting to opt for an oscilloscope with the highest specifications, focus on what you genuinely need for your projects. Consider both the upfront cost and the potential long-term value, such as the instrument's versatility, upgradeability, and maintenance costs.

      By carefully considering these five steps, you can select an oscilloscope that not only meets your project's current needs but also offers room for future growth and challenges.

      "For all used equipment, I offer my clients calibration and 1-year warranty." – Keysight Account Manager

      Experience Exceptional Value and Speedy Delivery With Keysight
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
      The Benefits of Choosing Refurbished Oscilloscopes

      Choosing refurbished oscilloscopes can offer significant advantages over purchasing new ones, from environmental benefits to cost savings, without compromising on functionality or support. Here's a closer look at these benefits:

      1. Environmental benefits: Opting for refurbished equipment plays a crucial role in reducing electronic waste and conserving resources. By giving a second life to oscilloscopes, you contribute to a more sustainable practice, minimizing the environmental impact associated with manufacturing and disposing of electronic devices.
      2. Warranty, calibration, and support services: Purchasing refurbished oscilloscopes from a reputable source often comes with warranties, calibration certificates, and support services similar to those offered with new equipment. This ensures that your device operates accurately and meets all manufacturer specifications, providing peace of mind and reliability.
      3. Cost-effectiveness and value for money: Refurbished oscilloscopes provide exceptional value for money. They offer the same advanced functionalities as the latest models but at a fraction of the cost. This cost-effectiveness allows for a higher or equivalent level of technology within budget constraints, making sophisticated equipment accessible to more users.
      4. Shorter lead times: Refurbished oscilloscopes typically come with shorter lead times compared to new orders. For projects with tight deadlines, this can be a critical factor, allowing quicker setup and commencement of work without the delays associated with manufacturing and shipping new equipment.

      Comparison Table: “Used” vs. “Premium Refurbished” Oscilloscopes

      FeatureUsed OscilloscopePremium Refurbished Oscilloscope
      WarrantyRarely offeredLike new
      CalibrationNot guaranteedFully calibrated to manufacturer's specifications
      Support ServicesLimited or noneComprehensive support and access to updates
      CostLower than newHigher than used but significantly lower than new
      ConditionVariableLike-new condition
      AvailabilityDepends on marketReadily available
      Lead TimeVariableTypically shorter than new

       

      While both used and premium refurbished oscilloscopes offer cost savings compared to new models, premium refurbished devices provide additional benefits. Keysight offers premium used devices that provide cost savings compared to new models. These devices come with warranty, calibration, and support services to ensure you get a reliable and customized device.

      "Customers come to us and buy used, because they get premium Keysight quality, with a lower price and we ship within 2 weeks. New equipment right now takes up to 14 weeks to ship." – Keysight Account Manager

      Conclusion: Optimize Your Diagnostics with the Perfect Oscilloscope Match

      Choosing the perfect oscilloscope is like picking the right key for a lock – it’s all about finding the best match for your specific needs. With so many types of oscilloscopes out there, from basic models perfect for learning the ropes to high-end devices designed for complex diagnostics, it's crucial to dive deep and understand what each type brings to the table. 

      This isn’t just about what you need right now; it’s about considering your future projects too. Think about things like how fast and detailed you need your measurements, how many things you want to measure at once, or if you need to take your gear on the go.

      It's all about balancing what you need with what each oscilloscope offers. Maybe you need something simple and portable, or perhaps you’re looking for a device that can give you deep insights with advanced features. Taking a moment to align your project’s demands with the right oscilloscope can save you time and hassle, ensuring that your work is not just done, but done well.

      In the end, the right oscilloscope doesn’t just make your job easier; it elevates your entire approach to diagnostics. So, take the time to choose wisely. Whether you’re working on straightforward tasks or navigating complex circuits, having the right tool in hand is key to ensuring reliability and top-notch results at every turn.

      Whenever You’re Ready, Here Are 5 Ways We Can Help You

      1. Browse our premium used network analyzers, oscilloscopes, signal analyzers and waveform generators
      2. Call tech support US: 1 800 829-4444. Press #, then 2. Hours: 7 am – 5 pm MT, Mon– Fri
      3. Talk to our sales support team by clicking the icon (bottom right corner) on every offer page
      4. Create an account to get price alerts and access to exclusive waitlists
      5. Talk to your account manager about your specific needs.