High Voltage Oscilloscope Probe: The Buying Guide

Your browser limits use of the Used Keysight Equipment website.
Please consider switching to a current version of Chrome, Firefox, Edge or IE11 to use this site.

Imagine you're tasked with maintaining the reliability of a high-power electrical substation. Here, every voltage fluctuation matters, and the difference between a routine day and a catastrophic failure could hinge on a few volts. 

In such a high-stakes environment, how do you ensure the accuracy and safety of your voltage measurements? This environment is precisely where a high-voltage oscilloscope probe becomes indispensable.

These probes are not just accessories but essential instruments for accurate, safe, and effective electrical and electronic measurements, especially in high-voltage environments like power generation, industrial systems, and automotive testing.

What is a High Voltage Oscilloscope Probe?

A high-voltage oscilloscope probe is a specialized tool designed to accurately measure high-voltage signals. It stands out from standard oscilloscope probes due to its ability to handle significantly higher voltage levels safely and effectively. 

These probes ensure that voltage measurements are accurate and secure, preventing damage to the oscilloscope and the user. 

With their enhanced safety features and precision, high voltage oscilloscope probes are indispensable in scenarios where standard probes fall short, particularly in industries where high voltage systems are the norm.

Fast Oscilloscope Delivery – So You Can Finish Your Project With Confidence
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
Types of High Voltage Oscilloscope Probes

Understanding the different types of high voltage oscilloscope probes is crucial for engineers to select the right tool for their specific measurement needs. Each type, be it differential, passive, or active, offers unique features and advantages suited to particular scenarios in electrical and electronic testing.

Differential Probes

Differential probes are designed to measure the difference in voltage between two points in a circuit. This design is crucial in isolating the specific part of the circuit you need to analyze, especially in complex electronic systems.

Design and Functionality

The core of a differential probe is its differential amplifier. This amplifier takes two inputs – one connected to each point in the circuit where the voltage difference will be measured. The probe then outputs a voltage proportional to the difference between these two points. 

This design is critical for accurate measurements in environments with high common-mode voltages, where traditional single-ended probes might be ineffective or dangerous.

Differential probes often come with high input impedance to minimize the loading effect on the circuit. They typically feature bandwidths that range from a few MHz to GHz, making them suitable for a wide range of applications. Additionally, many differential probes offer adjustable attenuation settings, allowing for flexibility in measuring a range of voltages.

Typical Use Cases

Differential probes are particularly useful when the signal of interest is not referenced to ground or when measuring between two points, neither of which is at ground potential. Common use cases include:

  • Power electronics: When dealing with inverter or converter circuits, differential probes can accurately measure the voltage across a semiconductor device, like an IGBT or a MOSFET.
  • Floating measurements: In applications like motor drives or power supplies, differential probes can safely measure voltages in a 'floating' circuit, where no part of the circuit is at ground potential.
  • Signal integrity and EMC testing: For high-speed digital applications, these probes help analyze signal integrity issues and electromagnetic compatibility (EMC) problems, where understanding the differential signal is crucial.

Preference Over Other Types

Differential probes are preferred over single-ended probes in high-voltage environments primarily because of their ability to provide accurate differential measurements without the risk of shorting the circuit to ground. 

They offer enhanced safety, especially when measuring high voltages not referenced to ground. Additionally, their high common-mode rejection ratio (CMRR) makes them ideal for noisy environments where precision is key.

Differential probes stand out for their unique design and functionality, making them an essential tool in any electrical engineer's toolkit, especially when dealing with complex, high-voltage systems.

Passive High Voltage Probes

Passive high voltage probes are another essential oscilloscope probe used extensively in various electrical and electronic applications. Their simplicity, reliability, and specific design features make them well-suited for certain high voltage measurement scenarios.

Basic Design and Operation

The basic design of a passive high voltage-probe involves a resistive voltage divider, which scales down the high voltage-signal to a level that an oscilloscope can safely and accurately measure. 

This voltage divider typically consists of high-resistance materials, ensuring the probe can handle high-voltage inputs while minimizing the effect on the tested circuit.

Passive high-voltage probes are characterized by their high input impedance, which is crucial for reducing the loading effect on the circuit under test. They are often designed to handle voltages ranging from hundreds to thousands of volts, making them suitable for various high voltage applications. 

These probes usually come with compensation adjustments that allow for fine-tuning to match the input characteristics of the oscilloscope, ensuring accurate waveform representation.

Typical Applications and Scenarios

Passive high-voltage probes are most useful in scenarios where high-voltage measurements are required, but the frequency range is not exceptionally high. Their typical applications include:

  • Power distribution systems: Passive probes provide a safe means to measure high voltage levels for monitoring and troubleshooting in power distribution networks.
  • Industrial equipment testing: In industrial settings, where machinery operates at high voltages, these probes are used for routine maintenance and fault diagnosis.
  • Educational and research labs: Due to their straightforward design and ease of use, passive high-voltage probes are commonly used in academic settings for teaching and research purposes.

Passive high-voltage probes are particularly favored in these scenarios for their durability and ease of use. They provide accurate measurements at relatively high voltages without needing external power or complex circuitry. This versatility makes them a reliable choice for many high-voltage measurement tasks.

Active High Voltage Probes

Active high voltage probes are sophisticated tools in the oscilloscope probe family, known for their precision and advanced features. These probes are designed for applications where high accuracy and wide bandwidth are required.

Construction and Working Principle

Active high voltage probes are characterized by their active electronic components, such as amplifiers and buffers, integrated into the probe itself. These components are powered, typically through the oscilloscope or an external power source, and are essential for the probe’s operation.

The key to an active probe's functionality is its ability to amplify the signal before it reaches the oscilloscope. This amplification is crucial in maintaining signal integrity, especially in scenarios involving high frequencies or very small signals. The active components also enable these probes to have a lower input capacitance compared to passive probes, which is beneficial for measuring high-speed signals as it minimizes the loading effect on the circuit.

Situations Where Active Probes Are Advantageous

Active high voltage probes shine in several scenarios where differential and passive probes might not be the best fit:

  • High-frequency measurements: In applications involving RF (Radio Frequency) or high-speed digital signals, active probes provide the necessary bandwidth and sensitivity.
  • Small-signal measurements in high voltage environments: Active probes can accurately capture small signals in the presence of large voltages, a situation where passive probes might struggle.
  • Precision testing and measurement: For work in R&D or laboratory settings, where precision and accuracy are paramount, the high fidelity of active probes makes them a preferred choice.
  • Dynamic range and low noise: Active probes typically offer a better dynamic range and lower noise floor, making them suitable for measurements where these factors are critical.

With their advanced features, active probes offer significant advantages in scenarios requiring high bandwidth, precision, and the ability to handle both small and large signals. Their specialized construction and operational capabilities make them an essential tool for engineers working on cutting-edge technologies, high-speed electronics, and precision measurement tasks.

Comparison Table of High Voltage Oscilloscope Probes

Feature/TypeDifferential ProbesPassive High Voltage ProbesActive High Voltage Probes
Design PrincipleDifferential amplifierResistive voltage dividerAmplifiers and active components
Power RequirementOften require external powerNo external power requiredRequire external power
Input ImpedanceHighVery highHigh
BandwidthModerate to highLow to moderateHigh to very high
Voltage HandlingHighVery highModerate to high
Common Mode RejectionExcellentNot applicableGood
Signal FidelityGoodModerateExcellent
ApplicationsPower electronics, floating measurements, EMC testingPower distribution, industrial equipment, educational labsHigh-frequency measurements, precision testing, small signal detection

How to Choose a High Voltage Oscilloscope Probe

Selecting the right high-voltage oscilloscope probe is critical for ensuring accurate and safe measurements. Key factors in determining the suitability of a probe for a specific application include voltage range, bandwidth, attenuation ratio, input impedance, accuracy, and application.

Voltage Range

Selecting the correct voltage range is vital for several reasons:

  • Safety: Ensures that the probe can handle the maximum voltage without damage to the probe or oscilloscope and without posing a risk to the user.
  • Accuracy: A voltage range that's too low can lead to probe overload and inaccurate readings. Conversely, a range that's too high may reduce sensitivity and measurement resolution.
  • Application suitability: The chosen voltage range should closely align with the expected voltage levels in your specific measurement scenarios to ensure precise readings.

Bandwidth

The importance of bandwidth in oscilloscope probes includes:

  • Frequency range accuracy: Bandwidth determines the range of frequencies the probe can measure accurately. It should be high enough to capture the highest frequency component of the signal.
  • Signal integrity: A bandwidth that is too low results in the attenuation of higher frequency components, leading to distorted and inaccurate signal representations.
  • Application relevance: This is especially crucial in high-speed digital and high-frequency analog applications, where capturing the entire spectrum of the signal is essential for accurate analysis.

Attenuation Ratio

The attenuation ratio of an oscilloscope probe is a crucial parameter that significantly influences measurement accuracy and probe performance. The attenuation ratio is the factor by which the probe reduces the amplitude of the signal before it reaches the oscilloscope. Common ratios include 10:1, 100:1, and 1000:1.

Significance

  • Signal scaling: A higher attenuation ratio allows the probe to measure higher voltages by scaling down the signal amplitude to a level the oscilloscope can handle.
  • Bandwidth and accuracy: The attenuation ratio can impact the bandwidth and accuracy of the probe. A higher ratio might lead to a lower bandwidth and reduced signal fidelity.
  • Selection criteria: Choose an attenuation ratio that matches the voltage levels you expect to measure. It's essential to balance the need for high-voltage measurement capabilities with the desire to maintain signal integrity.

Input Impedance

Input impedance is another critical factor in selecting an oscilloscope probe, affecting both the accuracy of measurements and the compatibility with the oscilloscope.

Role in Measurements

  • Loading effect: The input impedance of a probe affects the loading it places on a circuit. A high input impedance is generally preferred as it minimizes the loading effect, thereby reducing the impact on the circuit's operation and the distortion of the measured signal.
  • Signal integrity: Low input impedance can distort high-frequency measurements by affecting the signal's characteristics.

Probe-Oscilloscope Compatibility

  • Impedance matching: The input impedance of the probe should be compatible with the input impedance of the oscilloscope to ensure accurate signal transmission and measurement.
  • Considerations for selection: When selecting a probe, consider both the input impedance of the probe and the oscilloscope. This will ensure that the system as a whole functions optimally, providing accurate and reliable measurements.

Accuracy

Accuracy in high voltage oscilloscope probes is a critical factor that can significantly affect the outcomes in various measurement scenarios:

  • Measurement reliability: High accuracy ensures that the measurements are reliable and can be trusted for critical decision-making, especially in high-stakes environments like power generation or industrial control systems.
  • Fault diagnosis: In troubleshooting, accurate probes help to precisely pinpoint faults, leading to more effective and efficient repairs.
  • Research and development: In R&D, where new technologies are being tested, accuracy is essential for validating theories and experimental results.
  • Regulatory compliance: Certain industries require measurements that adhere to specific standards, where accuracy is not just a preference but a regulatory requirement.

Applications

Choosing the right probe based on specific measurement applications and requirements is essential for effective and accurate data collection. Here is a table outlining possible applications and the recommended types of probes.

Application AreaRecommended Probe TypeReason for Recommendation
Power Electronics (IGBTs, MOSFETs)Differential ProbesHigh common-mode voltage rejection and precise differential measurement
High-Speed Digital SignalsActive High Voltage ProbesHigh bandwidth and fidelity for accurate high-frequency measurements
Industrial Power SystemsPassive High Voltage ProbesHigh voltage handling capability and simplicity in rugged environments
Automotive ElectronicsDifferential ProbesAbility to measure across components with different ground potentials
Consumer Electronics TestingPassive High Voltage ProbesCost-effective for routine high voltage measurements
RF ApplicationsActive High Voltage ProbesEssential for accurately capturing very high frequency signals
Educational/Training LabsPassive High Voltage ProbesEasy to use and safe for educational purposes
Research and Advanced DevelopmentDifferential/Active ProbesRequirement for high accuracy, bandwidth, and specialized measurements

Additional Features and Accessories

High voltage oscilloscope probes come with a variety of additional features and accessories that can significantly enhance their functionality and ease of use. Here's an overview:

Additional Features

  • Readout options: Many probes include digital or analog readouts for more precise measurements, making recording and interpreting data easier.
  • Range selection: Adjustable range selection allows users to tailor the probe's sensitivity and scaling to the specific voltages being measured.
  • Compensation controls: These controls enable fine-tuning of the probe’s response, ensuring that it matches the oscilloscope's input characteristics for accurate measurements.
  • Probe calibration: Some probes offer built-in calibration features to maintain accuracy over time.

Common Accessories and Their Uses

  • Spring tips and hooks: For secure and stable connections to test points, especially in dense circuit layouts.
  • Ground leads: Essential for proper grounding, especially in high voltage environments to ensure safety and measurement accuracy.
  • Extension cables: Useful for increasing the distance between the probe and the oscilloscope, particularly in large-scale or hazardous environments.
  • Carrying cases: Protect probes from physical damage and environmental factors when not in use or during transportation.
  • Adapters: For connecting the probe to various types of connectors or ports, enhancing compatibility and flexibility.
  • Protective caps or covers: To protect probe tips from damage and users from accidental contact with high voltage points.

Incorporating these additional features and utilizing the appropriate accessories can improve the functionality, safety, and convenience of high-voltage oscilloscope probes in a wide range of measurement scenarios.

Balancing Budget and Performance

When investing in high-voltage oscilloscope probes, balancing the cost with the necessary performance and quality is a crucial consideration. Here are some insights on how to achieve this balance effectively.

Insights on Balancing Cost and Performance

  • Assess measurement needs: Clearly define the specific measurement requirements. Higher performance probes with advanced features are necessary for complex, high-frequency applications, but simpler tasks might not justify the additional expense.
  • Long-term value: Consider the longevity and durability of the probe. A higher initial investment in a quality probe can lead to cost savings in the long run due to fewer replacements and maintenance needs.
  • Brand and warranty: Opt for reputable brands that offer warranties and customer support, as this can be a sign of quality and reliability.

Advantages of Opting for Used or Refurbished Probes

  1. Cost-effectiveness: Used or refurbished probes often come at a significantly lower price than new ones, making them a budget-friendly option.
  2. Access to higher-end models: With a limited budget, buying used can provide access to higher-end models that would otherwise be unaffordable.
  3. Quality assurance: When purchased from a reliable source, used probes can offer comparable quality and reliability to new ones.

Key Benefits of Buying Used Probes from Keysight

  1. Certified quality: Keysight ensures that all used equipment, including probes, meets high-quality standards.
  2. Warranty and support: Keysight offers warranty and support services for used equipment, giving buyers peace of mind.
  3. Wide selection: A range of models and types are available, offering more options within the same budget.
  4. Cost savings: Significant savings compared to new equipment, allowing for the allocation of resources to other areas or additional equipment.

Key Insights from our Account Managers

  • Maximizing your budget: If you have allocated a budget for new equipment, consider exploring used equipment options from Keysight. This approach can significantly extend your budget, potentially allowing you to acquire more or superior equipment for the same investment.
  • Assured performance and quality: It's worth noting that many clients have reported high satisfaction with used equipment from Keysight. They find that these tools often meet, if not exceed, their performance and quality expectations, fitting well with their specific measurement requirements.

As you weigh your options, remember that opting for used equipment from a trusted brand like Keysight doesn't just offer financial benefits; it also assures you of reliability and quality, key factors in any measurement task.

We Help Engineers Meet Their Deadlines – Browse Our Offers
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
Matching Your High Voltage Probe With an Oscilloscope

Ensuring that your high voltage probe is compatible with your oscilloscope is essential for accurate measurements and optimal performance. Here are key aspects to check for compatibility and tips on proper usage and integration.

Key Things to Check for Compatibility

  • Connector type: Verify that the probe’s connector matches the input connectors on your oscilloscope. Common types include BNC, N-Type, or SMA connectors.
  • Impedance matching: Ensure the probe’s input impedance matches the oscilloscope’s input impedance (typically 50 ohms or 1 megaohm) to prevent signal distortion.
  • Bandwidth compatibility: The probe’s bandwidth should be equal to or greater than the oscilloscope’s to accurately capture the full frequency range of the signal.
  • Voltage range: Confirm that the probe’s voltage range is suitable for the signals you intend to measure and within the oscilloscope’s measurement capabilities.
  • Probe power requirements: Some active probes require a power supply, which should be compatible with the oscilloscope’s probe power output.

Correct Use and Integration of Probes with Oscilloscopes

  • Proper connection: Securely connect the probe to the oscilloscope, ensuring a stable and noise-free connection.
  • Compensation and calibration: Adjust the probe’s compensation (if available) to match the oscilloscope. This step is crucial for signal fidelity.
  • Setting up the oscilloscope: Configure the oscilloscope settings (like voltage/division and time/division) to suit the probe and the signal being measured.

Automatic Sensing and Scaling in Modern Oscilloscopes

Many modern oscilloscopes feature automatic sensing and scaling for probes. This technology allows the oscilloscope to detect the probe type and adjust its settings accordingly.
Automatic sensing simplifies setup and reduces the risk of incorrect settings, ensuring more accurate measurements. If your oscilloscope has this feature, ensure your probe is compatible with this functionality for a seamless and efficient measurement experience.

Working With High Voltage: Safety Considerations

Working with high voltage environments poses significant risks, making safety a top priority. Choosing the right high voltage oscilloscope probe is not just a matter of measurement accuracy but a critical safety decision.

Risks in High Voltage Probing

  • Electric shock: Direct contact with high voltage can lead to severe injury or fatality.
  • Equipment damage: Incorrect or mismatched probing can damage the oscilloscope and other equipment.
  • Arc flash and fire risks: High voltage can lead to arc flashes or fires if not handled correctly.

Essential Safety Measures and Protocols

  1. Proper probe selection: Use a probe rated for the voltage levels you will encounter. Ensure compatibility with your oscilloscope.
  2. Regular inspection and maintenance: Inspect your probes for wear, damage, and functionality.
  3. Use insulated tools: Always use insulated tools and wear protective equipment like gloves and safety glasses.
  4. Follow manufacturer's instructions: Adhere strictly to the usage guidelines provided by the probe manufacturer.
  5. Proper grounding: Ensure the probe and oscilloscope are properly grounded to avoid potential hazards.
  6. Stay within rated limits: Never exceed the voltage and frequency limits of your probes and oscilloscope.
  7. Training and awareness: Be trained in high voltage safety and stay aware of the surroundings while working.

Safety Standards and Ratings

  • IEC and ASTM standards: Familiarize yourself with international safety standards like IEC (International Electrotechnical Commission) and ASTM (American Society for Testing and Materials).
  • CAT ratings: Understand the Category (CAT) safety ratings of your equipment, which indicate the maximum voltage the equipment can safely handle in different environments.

Best Practices for Maintenance and Calibration

Maintaining and calibrating high-voltage oscilloscope probes is essential to ensure their longevity, accuracy, and safety. Here are the best practices to follow:

Maintenance Best Practices

  • Regular inspection: Routinely inspect probes for physical damage, wear, and tear, particularly on the cable, connector, and probe tip.
  • Clean regularly: Keep the probe clean, using appropriate cleaning agents to remove dirt and debris that might affect performance.
  • Proper storage: Store probes in a safe, dry place when not in use. Utilize protective covers and carrying cases to prevent damage.
  • Avoid stress: Avoid bending the cables excessively and protect the probe tip from impacts or harsh handling.
  • Follow manufacturer guidelines: Adhere to the maintenance guidelines provided by the manufacturer for specific probe models.

Calibration Best Practices

  • Regular calibration: Calibrate probes regularly to ensure accuracy. The frequency of calibration depends on usage, but annually is a common practice.
  • Professional calibration services: Use professional calibration services for precise and reliable calibration, especially for high-precision measurements.
  • Document calibration: Keep a record of calibration dates and results for future reference and compliance with any relevant standards or regulations.
  • Check for drift: Regularly check for any drift in the probe’s performance and recalibrate if necessary.

Importance of Regular Calibration

  • Measurement accuracy: Regular calibration ensures that the probes provide accurate measurements, which is crucial for reliable data and safe operations.
  • Compliance: Calibration ensures compliance with industry standards and regulations, particularly in critical applications.
  • Detecting faults: Regular calibration can help detect potential faults or wear in the probe before they lead to inaccurate measurements or equipment failure.

Keysight's Commitment to Calibration and Client Assurance

At Keysight, we are deeply committed to providing quality and assurance to our clients, especially when it involves used equipment. Our dedication to your satisfaction is reflected in the account managers’  approach to calibration:

"As part of our commitment to excellence, we offer our clients calibration and a 1-year warranty for all used equipment."

We are dedicated to ensuring that even our used equipment adheres to the highest standards of performance and reliability. By providing calibration services and a warranty, we ensure that you, our client, receive equipment that performs on par with new products.

Conclusion: Mastering High Voltage Measurements

Mastering high voltage measurements hinges on the careful selection of the right tools. This guide has provided a comprehensive overview of high-voltage oscilloscope probes, covering their types, key features, and applications. 

We've emphasized the importance of factors such as voltage range, bandwidth, attenuation ratio, and input impedance, highlighting the crucial role of accuracy and regular calibration in ensuring reliable measurements.

Selecting the right high-voltage oscilloscope probe is a decision that significantly impacts the precision, safety, and reliability of your measurements. Making an informed choice based on these considerations will ensure that you are well-equipped to handle the challenges of high voltage measurements, leading to successful and safe outcomes in your professional endeavors.

Whenever You’re Ready, Here Are 5 Ways We Can Help You

  1. Browse our premium used network analyzers, oscilloscopes, signal analyzers and waveform generators
  2. Call tech support US: 1 800 829-4444. Press #, then 2. Hours: 7 am – 5 pm MT, Mon– Fri
  3. Talk to our sales support team by clicking the icon (bottom right corner) on every offer page
  4. Create an account to get price alerts and access to exclusive waitlists
  5. Talk to your account manager about your specific needs.